Search results for: %20%EF%BF%BD%EF%BF%BD%EF%BF%BD%EF%BF%BD%20Ivermectin%2012mg%20Tablets%20Uk%20%EF%BF%BD%EF%BF%BD%EF%BF%BD%EF%BF%BD%20www.Ivermectin-Stromectol.com%20%EF%BF%BD%EF%BF%BD%EF%BF%BD%EF%BF%BD%20Ivermectin%20Tablets%20Otc%20%EF%BF%BD%EF%BF%BD%EF%BF%BD%EF%BF%BD%20Buy%20Stromectol%2012mg%20Canada%20%7C%20Ivermectin%2012%20Mg%20Over%20The%20Counter%20Canada
Depth and Accessibility
October 16, 2019This month is National Disability Employment Awareness Month, which is the perfect time to discuss some accessibility solutions where depth is or could be potentially helpful. Depth cameras are designed to help computers understand and interpret the world, which makes them ideal devices for offloading a variety of tasks from and for humans. In the…
Read MoreArt and Interactivity in the Touch-free age
May 20, 2020In a time when we are all increasingly spending much of our free time at home for the near future, and socially distancing when we do return to public life, it’s hard to see what our future entertainment options look like from here. The drive-in movie theater is a great example of contact-free entertainment that…
Read MoreThe Beginner’s Guide to 3D Film Technologies
January 17, 2019With growing interest in new immersive entertainment platforms like Virtual and Augmented reality, 3D photos on Facebook, 360° videos on YouTube and more, it can be hard to understand the nuances and differences between all of these different photo and video technologies, and even harder to know where to start if you’re someone who wants to create something new.
Read MoreCase study: Visual-Inertial Tracking
February 22, 2019Intel RealSense Tracking Camera T265 Buy Case study Robust Visual-Inertial Tracking from a Camera that Knows Where it’s Going The Intel® RealSense™ Tracking Camera T265, powered by the Intel® Movidius™ Myriad™ 2 vision processing unit (VPU), delivers 6DoF, inside‑out tracking for highly accurate, GPS-independent guidance and navigation for robots and other mobility‑focused implementations. Gartner identifies “autonomous things” as Trend Number 1…
Read MoreFAKRA/GMSL Q&A
September 21, 2022FAKRA/GMSL Q&A 1. What is Intel® RealSense™ Depth Camera D457? The Intel® RealSense™ Depth Camera D457 features our longest range widest field of view global shutter camera with a GMSL serializer and FAKRA connector. 2. What is the size of the peripheral? Based on the D455 camera, the peripheral dimensions are 124 mm (X) ×…
Read MoreCalling all Creators and Makers, introducing the Muse Vision
April 18, 2019The modern laser cutter provides affordable and easy to use technology that allows creation and replication of beautiful art or complex physical products. Muse laser cutters from Full Spectrum laser put state-of-the art engineering in a full-featured compact package suitable for the home maker or space strapped startup.
Read MoreDepth and Gaming
November 11, 2020Depth Cameras and Gaming For many people, their first introduction to a depth camera was with the release of the original Microsoft Kinect. The Kinect was a depth camera that utilized coded or structured light depth sensing techniques to evaluate the scene in front of the camera, allowing players to interact with games without the…
Read More