Search results for: 🙂 Is Ivermectin Safe For Children 🔰 www.Ivermectin4Sale.com 🔰 Can You Give Dogs Ivermectin 😄 Ivermectin Dosage For Dogs Intestinal Parasites , Cost-effectiveness Of Ivermectin
Depth and Healthcare
February 19, 2020Between 2015 and 2030, the number of people in the world over 60 is expected to grow to as many as 1.5 billion people. By 2050, that number will jump to two billion. In the USA alone, this number is expected to be as many as 100 million people by 2060. There are many challenges…
Read MorePractical 3D Scanning with Dot3D Pro
December 13, 2018What is 3D Scanning? 3D scanning has come a long way since the first ever object to be ‘scanned’ using students, paint and rulers. Even with the advent of more advanced techniques in the mid-1990s, 3D scanning was still slow and limited to small objects that could fit on a turntable – often also constrained by…
Read MoreUnreal Engine 4 with Intel® RealSense™ Technology
November 27, 2018One of the most constantly evolving and frequently cutting edge areas of technology and innovation is gaming. Whether that’s pushing compute to the limit with the latest first person shooter, or ever-more-real virtual worlds, gaming leads the way. Since many games use similar features regularly, game engines are used to speed development – for example,…
Read MoreHundreds of thousands of people experience an out-of-hospital cardiac arrest every year. In Europe alone, that number is around 275,000. In the USA, more than 350,000 cardiac arrests occur outside of the hospital each year. While emergency responders do everything they can to respond to these life threatening situations as rapidly as possible, survival rate…
Read MoreArt and Interactivity in the Touch-free age
May 20, 2020In a time when we are all increasingly spending much of our free time at home for the near future, and socially distancing when we do return to public life, it’s hard to see what our future entertainment options look like from here. The drive-in movie theater is a great example of contact-free entertainment that…
Read MoreDepth Camera D555 with Power over Ethernet (PoE) interface, IP65, IMU, RGB, ROS2 support
May 12, 2025Intel® RealSenseâ„¢ Depth Camera D555 Coming soon 3D Computer Vision Powered over Ethernet Intel® RealSenseâ„¢ Depth Camera D555 introduces Power over Ethernet (PoE) interface on chip, expanding our portfolio of USB and GMSL/FAKRA products. Coming soon New SoC Generation D555 is the first camera powered by the new Intel RealSense Vision SoC V5. Built-in IMU and…
Read More3D Scanning for Custom Footwear and Orthotics
September 11, 2023Case Study: Aetrex Download 3D scanning for custom footwear and orthotics Challenge Solution Results Challenge Accurately develop a three-dimensional profile of each customer’s foot, including measurements of the length, width, instep, arch height, girth, arch type, and other parameters. Solution Intel® RealSenseâ„¢ depth camera D415 puts an Intel module and vision processor into a small…
Read More