Search results for: 💛 Order Ivermectin Otc ☑️ www.Ivermectin4Sale.com ☑️ Buy Ivermectin 6mg Online Canada 🍆 Ivermectin For Humans Dosage Uk . Ivermectin 3 Mg Tablets Uk
Are we living in the future? Science fiction movies have long made us elaborate promises about the future – both good and bad. Sometimes those promises are about big, society changing things like space travel or teleportation, but there are plenty of smaller scale predictions too, inventions that make up the fabric of these future…
Read MoreBeginner’s guide to depth (Updated)
July 15, 2019We talk a lot about depth technologies on the Intel® RealSense™ blog, for what should be fairly obvious reasons, but often with the assumption that the readers here know what depth cameras are, understand some of the differences between types, or have some idea of what it’s possible to do with a depth camera. This…
Read MoreWhat does depth bring to Machine Learning?
May 2, 2019What is Machine Learning? Before we start any discussion about Machine Learning, we should discuss what it is. Machine learning makes use of algorithms and statistical models to make predictions and guesses about data. It’s sometimes also referred to as “artificial intelligence” although machine learning is generally about performing a specific task or function, rather…
Read MoreCalling all Creators and Makers, introducing the Muse Vision
April 18, 2019The modern laser cutter provides affordable and easy to use technology that allows creation and replication of beautiful art or complex physical products. Muse laser cutters from Full Spectrum laser put state-of-the art engineering in a full-featured compact package suitable for the home maker or space strapped startup.
Read MoreArt and Interactivity in the Touch-free age
May 20, 2020In a time when we are all increasingly spending much of our free time at home for the near future, and socially distancing when we do return to public life, it’s hard to see what our future entertainment options look like from here. The drive-in movie theater is a great example of contact-free entertainment that…
Read MoreDepth Camera D456
October 9, 2023Intel® RealSense™ Depth Camera D456 Buy An IP65 rated long range depth camera. The Intel® RealSense™ Depth Camera D456 is based on our longest range D455 USB popular camera with 3 global shutter sensors and IMU. The D456 has an IP65 rated enclosure which is dust tight and protected from projected water. Buy FOV 87° × 58°…
Read MoreDepth Camera D455f
July 9, 2023Intel® RealSense™ Depth Camera D455f Buy Long range with IR Pass Vision D455f features our long range D455 with an IR pass filter. The addition of an IR Pass Filter over the lenses resolves repetitive pattern and false object detection due to light reflections. Buy FOV 87° × 58° Ideal Range 0.6 m to 6 m Global…
Read More