Search results for: %20%EF%BF%BD%EF%BF%BD%EF%BF%BD%EF%BF%BD%20Ivermectin%2012mg%20Tablets%20Uk%20%EF%BF%BD%EF%BF%BD%EF%BF%BD%EF%BF%BD%20www.Ivermectin-Stromectol.com%20%EF%BF%BD%EF%BF%BD%EF%BF%BD%EF%BF%BD%20Ivermectin%20Tablets%20Otc%20%EF%BF%BD%EF%BF%BD%EF%BF%BD%EF%BF%BD%20Buy%20Stromectol%2012mg%20Canada%20%7C%20Ivermectin%2012%20Mg%20Over%20The%20Counter%20Canada
Depth Camera D415
January 7, 2019Intel® RealSense™ Depth Camera D415 Buy Depth Camera D415 The Intel® RealSense™ D415 has a standard field of view well suited for high accuracy applications such as 3D scanning. With a rolling shutter on the depth sensor, the D415 offers our highest depth quality per degree. Precision and Accuracy When accuracy is the most important factor for your solution, the D415 is the perfect choice.…
Read MoreAethon: Industry-Changing Mobile Delivery Solutions
May 18, 2020Case Study: Aethon Download How Intel® RealSense™ depth sensing technology is helping Aethon create industry-changing mobile delivery solutions. Challenge Solution Results Challenge Healthcare, manufacturing, and hospitality industries face a costly challenge- moving things from place to place efficiently. Many mobile delivery robots require multiple sensors and complicated programming, and this means a higher bill of materials…
Read MoreFAKRA/GMSL Q&A
September 21, 2022FAKRA/GMSL Q&A 1. What is Intel® RealSense™ Depth Camera D457? The Intel® RealSense™ Depth Camera D457 features our longest range widest field of view global shutter camera with a GMSL serializer and FAKRA connector. 2. What is the size of the peripheral? Based on the D455 camera, the peripheral dimensions are 124 mm (X) ×…
Read MoreLidar Camera
November 18, 2019Intel® RealSense™ LiDAR Camera L515 Intel® RealSense™ LiDAR Camera L515 Introducing the world’s smallest high‑resolution LiDAR depth camera. Intel® is proud to introduce a revolutionary solid-state LiDAR depth technology designed for indoor applications. The first product in the new LiDAR depth family, the Intel RealSense LiDAR Camera L515 is perfect for applications that require depth data at high…
Read MoreDepth Camera D455
June 5, 2020Intel® RealSense™ Depth Camera D455 Buy What is GMSL/FAKRA? Intel RealSense Depth Camera D457 Watch the replay Twice the range. Better performance. See further. The D455 extends the distance between the depth sensors to 95 mm which improves the depth error to less than 2% at 4 m. Compare cameras A perfect pair. To improve the RGB image and the correspondence between the…
Read MoreAutomated Warehouse Order Fulfillment
June 25, 2020Case Study: RightHand Robotics Download How RightHand Robotics is using Intel® RealSense™ computer vision technology to revolutionize automated warehouse order fulfillment. Challenge Solution Results Challenge Warehouse managers are looking for a comprehensive, predictable, adaptable, piece‑picking solution that will allow them to automate ecommerce order fulfillment, but traditional factory robots programmed for just one task aren’t up to the challenge. Solution…
Read MoreSoftware for Intel RealSense
February 14, 2019Software for Intel® RealSense™ Technology We’ve teamed up with the best depth sensing software developers to provide you an outstanding result. 3D Scanning Background segmentation Digital art Digital signage Eye tracking Gesture recognition and hand tracking Machine vision Measurement People tracking Retail Skeletal tracking 3D Scanning DotProduct develops high performance, easy-to-use solutions for capturing 3D data. Their self-contained handheld 3D scanning products have revolutionized…
Read More